Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21415
  • Release Date : 2018/08/22 16:27
  • Print

Long wire to terminal FM

I am considering to connecting a frequency meter to the terminal FM. How can I install the HMI (Human Machine Interface) at a remote location?
(Approximately 100 m)
Category : 

Answer

Although you can connect an analog or digital indicator to the terminal FM, use an analog indicator since the wiring length is long. (The maximum wiring length is 200 m for the analog indicator and 50 m for the digital indicator.) Use a twisted pair or shielding wire of 0.3SQ or higher for connection.
Use an analog indicator with an ammeter of 0 to 1 mA and indicator using frequency scale display.
We offer the YM206RI 1 mA frequency meter as an option.
Product Name
Inverter, magnet motor drive
Series
Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries